Select a Nameplate Datasheet as the data source

The
Nameplate Datasheet
data source derives motor attributes from a motor nameplate and datasheet.
To select a Nameplate Datasheet as the data source:
  1. In the
    Axis Properties
    dialog box, in the
    Categories
    pane
    ,
    click
    Motor
    .
  2. In the
    Motor Device Specification
    area, from the
    Data Source
    list, click
    Nameplate Datasheet
    .
  3. From the
    Motor Type
    list, click a motor type. The motor information boxes are initialized to defaults.
  4. In the
    Nameplate/Datasheet - Phase to Phase
    parameters area, reference the motor nameplate datasheet to enter the parameter information for the motor and click
    Apply
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.