DC Bus page
Use the settings on the
DC Bus
page to configure DC Bus functionality for a regenerative converter. Use the page to:- Configure the load capacitance of the DC Bus.
- Configure the total system capacitance of the DC Bus.
The
DC Bus
page is available when, on the General
page, the Axis Configuration
is set to Regenerative AC/DC Converter
or Low Harmonic AC/DC Converter
.
TIP:
To open the DC Bus page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, clickGeneral.
- In theAxis Configurationbox, selectRegenerative AC/DC ConverterorLow Harmonic AC/DC Converter.
- InCategories, selectDC Bus.
Parameter | Description |
---|---|
External Bus Capacitance | Specifies the external DC Bus capacitance when the associated converter or drive is acting as a Bus Master, supplying DC Bus power to one or more common bus followers. This value is also applicable to standalone converters that allow connection to an external capacitor. The default is 0.0 f. |
Converter Bus Capacitance | Shows the bus capacitance of the regenerative converter. |
Total Bus Capacitance | Specifies the combined capacitance of the regenerative converter and external DC Bus capacitance. The default is 0.0 f. |
System Capacitance | Specifies the total system capacitance of the DC Bus. This scaling gain value converts voltage rate commanded by the bus voltage control loop into equivalent active current, expressed as a percent of the converter’s current rating. The default is 0.0 %Rated (Volts/s) This parameter is only available when the Converter Configuration on the General page is set to Bus Voltage Control . |
Provide Feedback