Loading
Blog
Recent ActivityRecent Activity
3 minute read

Gain Flexibility, Productivity with Modern Batch Systems

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Gain Flexibility, Productivity with Modern Batch Systems hero image

Increasing consumer demands have brought the need for improved, more flexible production solutions to the forefront. From handling a larger variety of products to requiring easier and more frequent changes throughout production, chemical companies are looking for ways to increase operational flexibility.

The utilization of a modern batch control system is helping these companies achieve more flexible, productive and efficient chemical operations. Batch systems sequence the same set of production equipment in different ways, according to specific recipes, which produce different end products.

Having a system that allows operators to easily and fully control these recipes is key to achieving the flexibility required in today’s environment. Below are some improvements that companies have seen with the implementation of a modern batch system:

  • Increased yields
  • Decreased unplanned downtime
  • Enforced procedures
  • Reduced batch cycle times
  • Enhanced reusability

Traditional batch systems are not able to meet the increasing needs of chemical companies and their consumers. These systems cause production issues like unnecessary nuisance pop-up alerts, lack of recipe-based automation and complex changeover operations.

All of these can lead to decreased product quality and yield and increased batch cycle times, reducing overall plant performance. A modern batch system, however, can provide significant production benefits.

Our batch control solutions provide a flexible control environment to help you meet your demands for increased production and improved yields. Learn more here.

Flexibility and Quality Control

A modern batch system brings a new level of flexibility to today’s chemical plants. The system enables operators to easily change recipes with minimal manual interaction. This allows for quicker and more frequent changeovers, effectively allowing companies to produce batches in a variety of sizes. 

Specialty chemical producer DuPont implemented a modern batch system to take the place of their obsolete, traditional system. The company is now able to save significant time and effort, as they only have to configure one new phase when making changes to their solvent recipe.

They are now able to reuse this configuration. As noted above, a modern batch system allows producers to follow the same procedures and configurations repeatedly with less operator intervention. This reduces variability and error throughout production. In total, this drives faster manufacturing processes, increases flexibility and improves product quality.

Variability and Reliability

A traditional batch system requires the full process sequence to be designed and laid out from the batch server. Interaction with data and decision-making takes place before the transition to each new process step. Operators are not able to receive data throughout the operation in real time. A modern batch system provides operators with batch execution data in real time, allowing for a continuous evaluation of batch parameters and providing valuable insights into the process.

In the modern system, portions of the batch sequence run directly in the controller, allowing it to perform sub-second transitions from one batch process step to the next. With a traditional batch system, these sequences run in a server. This requires the server to continuously communicate with controllers to execute actions, thus increasing the time required to execute these transitions. Time and effort are saved when these transactions happen on the controller, independent from the server. 

Scalability

When adding new process equipment to your production line, additional programming makes for a long and challenging process.

One example: When a plant moves from a single mixing unit to multiple units. A modern batch system significantly reduces the engineering effort to implement these changes. By utilizing the existing information in the system, new units can be added with the same capabilities of the existing unit – therefore existing recipes and sequences can be executed using the new equipment.

Plus, if there are minor differences in the operation of the units, a portion of the sequence can be executed on the controller, which again allows for fewer changes to the existing recipes and sequences. Not only does this save time, it reduces engineering costs.

Skid vendors and OEMs can also benefit from the scalability of a modern batch system. These vendors can provide units that include phases and even sequences that can be integrated into the server-based batch system.

These phases and sequences defined on the controller can then be executed from the supervisory level. This means vendors can provide additional value to their end customers while still maintaining the ability to determine the capabilities of the units they are providing.

With the use of a flexible, modern batch system, chemical producers can increase productivity and keep up with consumer demands. Not sure where to get started? Learn more here.

Published May 22, 2019

Topics: Chemical

Jamey Geer
Jamey Geer
Batch Product Manager, Rockwell Automation
Jamey has been working with Rockwell Automation for over 15 years. He spent several years applying Rockwell Automation technologies and developing automation systems before transitioning into Commercial Engineering. He took over as the Product Manager for Batch Control in December of 2018.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Gain Flexibility, Productivity with Modern Batch Systems Chevron RightChevron Right