Loading
Blog
Recent ActivityRecent Activity
5 minute read

Medical Devices: Rapidly Adapting to Meet Demand in a Crisis

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Medical Devices: Rapidly Adapting to Meet Demand in a Crisis hero image

Global crises play havoc with demand patterns. The markets for certain products collapse overnight while demand for other goods skyrockets. At the time of writing, we are in the middle of the 2020 COVID-19 pandemic, and much of the upheaval we are experiencing is understandably centred on medical devices.

Inevitably, equipment to treat and contain the virus – such as PPE, test kits, ventilators and respirators – are seeing unprecedented demand. This is in stark contrast to devices and equipment for non-essential surgeries, such as hip and knee replacements.

But this is just one example. If the pandemic is showing us anything, it is that demand patterns cannot be taken for granted. Medical device companies must have strategies in place to enable both business continuity and some degree of flexibility to meet changing demands, even after the current pandemic has run its course. I believe the digitally transformed manufacturer will be best positioned to succeed in this environment.

Key Challenges for Medical Device Manufacturers

The medical device supply chain is currently under huge pressure, and any disruption to one link will send ripples through all the others. As demand increases, the opportunity for one of the links to fail also increases, threatening to impact delivery, manufacturing capacity and, ultimately, the patient.

This demand can’t always be met from elsewhere, either. Alongside the complexities presented by the technical, specialised nature of medical devices, the high level of regulation they are subject to is a challenge few from outside the industry can quickly master. That’s why the majority of high-profile ‘pivots’ from manufacturers in automotive and consumer goods that grabbed the headlines in the early weeks of the pandemic have come to little, and even life sciences manufacturers have had to overcome significant challenges to pivot production.

Additionally, the relaxing of certain standards to allow for the mass production of PPE has resulted in unfit-for-purpose products entering the supply chain. The NHS was forced to impound 400,000 protective gowns manufactured in Turkey after they failed to meet UK standards

– Ireland experienced a similar problem
with PPE from China.

The Socially Distanced Factory

Medical device companies are taking a double hit in the current crisis: not only are they facing pressure to increase production volumes, but social distancing requirements to ensure staff safety are threatening to disrupt normal operations.

In order to adapt to the reality of the socially distanced factory, shifts must be staggered. If just one person on the line shows symptoms, the entire shift will need to self-isolate. The manufacturer may then need to rapidly onboard a new team that is unfamiliar with the manufacturing processes.

Crisis measures can also have a severe impact on areas such as maintenance and repair of critical manufacturing equipment. Much of this equipment originates overseas, with experts often flown in to attend to it. But today, such experts must quarantine for up to 14 days upon entering a country prior to being able to travel to site, leading to expensive downtime, extra costs and inefficiencies.

Digital Transformation as the Solution

As we enter a period of sustained uncertainty, the companies that have set themselves up to quickly adapt their production and working practices are better positioned to weather these new challenges. What these companies often have in common is a high degree of digital maturity.

In some organisations, digital technologies such as augmented reality (AR) and advanced simulation tools are already providing solutions to many of the issues introduced by the socially distanced factory. By capturing manual activities in the virtual environment, they enable rapid knowledge transfer to train new shifts, reducing onboarding and training time, and bridging gaps in expertise within new or recently redeployed teams.

AR can also be used to guide operators or maintenance personnel, enabling remote experts to help local resources perform the critical tasks and maintenance required to recover from unplanned downtime situations. Meanwhile, simulation tools enable engineers to map equipment layouts and simulate the impacts on productivity and throughput that would arise as a result of layout changes. In this way an optimal solution can be found without the need for experts to make physical adaptations on-site.

AR is a quick and easy-to-implement technology. But to meet the greater challenges presented by rapid changes in demand, manufacturing processes and supply chain visibility, a more holistic digital transformation is often required.

For example, businesses that have digitalised their end-to-end supply chain and are utilising disruptive technologies such as AI and advanced analytics can already model for spikes in demand, pinpoint and account for disruption, and automatically feed this information into internal forecasts. These connected operations also enable them to realise cost savings and increased control without opening them up to the vulnerabilities engendered by a fully consolidated supply chain.

Once they have achieved a greater level of visibility and control, organisations can work on their own link within the chain, deploying flexible manufacturing technologies that allow them to scale their output and more easily pivot to create new lines or products without time-consuming and costly manual changeovers. The net result is an end-to-end supply chain that is better equipped to adapt to the spikes and troughs in demand that come in times of crisis.

Starting the Transformation Journey

Although the pandemic has put many activities on hold, manufacturers can still take the first steps towards digital transformation now. We have supported numerous companies on their digital transformation journeys, and have identified a number of critical success factors on the way.

Firstly, companies that understand their core objectives and outcomes are more successful. Having clear goals and KPIs at the outset enables the progress of any initiative to be measured. The organisation must be aligned around these goals, and must understand the processes required to achieve them.

Secondly, there must be a full examination of the digital maturity level of current manufacturing operations. An organisation needs to understand what is installed in its plants and assess the maturity of its infrastructure, processes, technology and people if it is to plan and achieve a digital transformation. Following this assessment, an analysis of the technology available in the market needs to be conducted, and an understanding of the value it will bring to the company should be reached.

Finally, successful companies secure buy-in and senior-level sponsorship for their proposed digital projects. Such projects require cooperation across many business units; support from leadership is essential to driving out silo mentality and encouraging different parts of the business to work together.

Meeting Demand in the New Normal

There’s no end in sight for the current crisis, at least in the immediate future. Instead, manufacturing and markets will slowly settle into what is being called ‘the new normal’, where ‘normality’ refers to a state of perpetual change and uncertainty. Medical device manufacturers must therefore put themselves in a strong position to respond to constantly shifting market conditions.

The key to successfully navigating these uncertain times is digital transformation. Those with a comprehensive view of the entire product lifecycle across their operations, manufacturing networks and supply chains will be better placed to deal with dramatic fluctuations in demand. This makes it all the more vital for those who haven’t done so to take the crucial first steps now.

Agility, flexibility and security are defining modern life sciences operations. Join our Life Sciences Industry Forum webinar series to see how you can give the market what it needs.

Published June 15, 2020

Topics: Life Sciences

Billy Sisk
Billy Sisk
Life Sciences Industry Manager EMEA, Rockwell Automation
Billy has worked extensively both in automation and IT and is responsible for Rockwell Automation’s life science market strategy across EMEA. Through his high performing team, Billy helps pharmaceutical manufacturers bring innovative treatments to patients faster, while improving quality, yield and product security.
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Medical Devices: Rapidly Adapting to Meet Demand in a Crisis Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose