The new system had to seamlessly integrate the previous connections with the field devices (valves, hydraulic systems, etc), thus avoiding a longer shutdown due to moving cables and wires from the old panel to a new one. Integration of all the existing metering systems was also a requirement – the loading meters and scales. This had to be done via a serial interface.
Solution:
According to George Marinescu, control engineer Smartech Automation SRL: “The four loading ramps are now each controlled and monitored by four operators, each with its own high-end operator interface. A primary server hosts the application, which is served to the operator panels using dedicated software. Gateway software is used to interface with the terminal management application as an OPC server.”
The operator stations are used for the loading process control (positioning of the loading tube) and monitoring (real time loading data, such as mass, volume, density, for all the meters and scales for a given ramp/station), allowing the operator to now work in one of two modes:
- Online mode – All the loading data is received from the terminal management application and after loading, all the resulting loading data is sent back (loaded mass, volume, average density, temperature, meter used, batch number, etc).
- Fall-back or offline mode – The operator can access tables, which allow them to fill in the data normally received from the terminal management application. The resulting final data is then logged in an SQL database, saved in a queue to send back to the terminal application, when it becomes available again. The offline mode also allows for printing of reports and data retrieval. Thus, the offline mode replicates some of the functions of the terminal management application when it is not available.
Marinescu continues: “The previous application’s functions were split and some moved on the PLC level (meters and scales communication, loading steps, meter interlocks) while others were implemented in the software application (loading results reporting, SQL archiving).
“The PLC racks were left into place due to commissioning time constraints,” he adds, “but the CPUs were replaced with Allen‑Bradley® 1747-AENTR Ethernet adaptors and the PLC code migrated and adapted into new mid-range programmable automation controllers (PAC).”
Four MVI69L-MBS Modbus Serial Lite Communication Modules from Prosoft Technology, a Rockwell Automation Encompass™ Product Partner were also used – mounted on the PAC chassis – to deliver serial communication capabilities.
Results:
The new system was seamlessly interfaced with the terminal management application, delivering the easy exchange of necessary data between the two systems. All the existing functions are replicated in the new system, this time on a more open platform, comprising operator interfaces and PACs.
This new platform allows for the easy addition of new features (new products to be loaded, changes and improvements of the loading process, addition of new meters, etc) and time is now no longer being lost on tasks such as manual data input or managing paper reports.
Marinescu explains: “We are working on a new system for two more loading ramps, for the same client, but this time the ramps are new. The core system will have pretty much the same functionality as the modernised one; however, since the ramps are new and the commissioning time constraints are not as great, we are able to design a more advanced control system, with brand new automation panels. The new system uses the same server/software/interface solution, alongside redundant High-end PACs.
“Other ongoing projects we are working on using Rockwell Automation products include a demineralized water finishing station for a thermoelectrical plant, using redundant high-end PACs, high end HMI software and hardware solutions and process I/O modules.”