Pane bar
Use the icons on the pane bar to perform certain tasks:
Item | Description |
---|---|
Left panes . Toggle the panes on the left side of the user interface. | |
Explorer . Toggle the selected Explorer pane. | |
Right panes . Toggle the panes on the right side of the user interface. | |
Toolbox . Toggle the Toolbox of instructions to add to a ladder diagram and an Add-On Instruction. | |
Properties . Toggle the Properties pane for the selected element. | |
Bottom panes . Toggle the panes at the bottom of the user interface. | |
Output . Toggle the error, warning, and information messages that appear for the routines and instructions in the project. |
Provide Feedback