Pull changes from the remote repository

Update your local workspace when changes are made to the remote repository. Pull changes when the status bar displays
Remote changes available
. When you pull changes, the project copy in your local workspace is updated with changes made to the project in the remote repository. Any conflicts between the two versions of the project appear for you to choose which version of a change to keep.
IMPORTANT: Pulled changes cannot be undone. Pull changes only if you want to make the project in your local workspace the same as the project in the remote repository.
TIP: The number in the icon identifies the total commits made by other users sharing the project (remote commits).
Prerequisite
  • If you made changes to the local project, commit your changes before pulling remote commits. Select Commit icon
    Commit
    . In the open project, if
    Remote changes available
    appears in the status bar, select Pull icon
    Pull
    or select
    File > Source control > Pull
    . The open project updates with any changes made to the shared project on the remote repository.
    TIP: If the remote version of the project has changes to the same content as the local project version,
    Manage conflicts
    opens.
To pull changes from the remote project
:
  1. If
    Manage conflicts
    opens, use:
    • Status
      to identify if the file contains conflicts.
    • Path
      to reference the files that have conflicts.
    • Conflicts
      to identify the number of conflicts in a file and
      Total conflicts
      to identify all the known conflicts.
  2. Select each conflict in the table and then select an option above the changed code for the conflict:
    • Accept local change
      . Discard the change made to the remote version of the project and accept the change that appears in the LOCAL CHANGES row of code. This option updates the remote version of project with the change made to the local version of the project.
    • Accept remote change
      . Discard the change made to the local version of the project and accept the change that appears in the REMOTE CHANGES row of code. This option updates the local version of the project with the change made to the remote version of the project.
    • Accept both changes
      . Apply the changes in both the LOCAL CHANGES and REMOTE CHANGES rows of code.
      TIP: If another user deletes a file remotely from the shared project while
      Manage conflicts
      is open,
      Remote changes available
      appears again.
  3. (optional) After you accept changes, the
    Revert
    button is enabled. Select
    Revert
    if you want to return the files to the previously applied or committed changes.
  4. To manage any remotely removed files, select Pull icon
    Pull
    again and then in the first
    Keep file
    column of
    Manage conflicts
    , either:
    • Select the checkbox to keep the file that the other user removed remotely.
    • Leave the checkbox cleared to remove the file from your local project as well.
  5. When all conflicts are resolved, select
    Accept
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.