Delete a program
A program contains routines, including a main routine and tags.
Delete programs from the
System
explorer. Deleting a parent program deletes the programs the program contains. - On the explorer bar, selectSystem.
- Right-click a program and selectDelete. The messageAre you sure you want to delete this programappears.
- SelectDelete. The program no longer appears inSystem.
Provide Feedback