Change the properties of a routine
Change the properties of a routine to view and change the name and descriptions of the routine.
To change the properties of a routine
- On the explorer bar, selectSystem.
- InSystem, expand theFactoryTalk Smart Objectand program.
- Double-click a routine preceded by
.
- In the open routine, change the properties:
- Routine. Enter a new name for the routine.
- Description. Enter a new description for the routine.
- In Program. The program in which the routine exists. This property is read-only.TIP: If thePropertiespane for the routine does not open, place the title bar of the routine in focus and then selectProperties.
Provide Feedback