Configure a dropdown button
Configure a
Dropdown button
object by linking it with a container object type.- InProject view, create a container object type to display when you select the dropdown button.For more information, see Create a graphic object type.For example, create a panel type.
- InProject view, inUI, right-click a container and select .
- InProperties, create a dynamic link between thePanelproperty and the container object type.For more information about dynamic links, see Create dynamic links.
dropdown
dropdown button
Provide Feedback