Apply a control style to a graphic object
Apply a control style to a specific graphic object instance or type. Control styles overwrite the global style.
Prerequisites
- Configure a stylesheet to contain multiple styles for a given graphic object type. See Configure a style sheet.For example, add a custom style for switch objects.
- To apply a style to a graphic object
- InProject view, select a graphic object or a graphic object type.For example, select a button. Button objects come with multiple predefined control styles.
- InProperties, inStyle, select the drop-down arrow after the value and select the style to apply.For example, selectAccent.
The graphic object or graphic object type uses the selected control style.
Provide Feedback