Assign a role to a user or group
Assign roles to users and groups to create a hierarchy of roles with assigned rights and privileges.
- In the main toolbar, selectand then selectOpen dashboard pageManage users and groups.
- On the dashboard page, either:
- UnderRoles,drag a group onto a user underUsersor onto a group underGroups. You can also drag a user or group onto a role. Hold downShiftorCtrlto select and drag consecutive or multiple selections.
- Select one or more roles, selectAssignto users or groups, select the users and groups, and then selectApply.
TIP:appears next to a group or role that is already assigned to a role. You can assign the role to a user or group from
Project viewby dragging the role to the user or group inProject view.
The role appears assigned to the user or group on the dashboard page.
Provide Feedback