- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Converter Output Attributes
These are the converter output related attributes associated with Motion Control Axis.
Converter Output Current
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | T | REAL | - | - | - | Amps |
The Converter Output Current attribute is the output current generated by the Bus Converter. A positive value indicates current flow out of the converter, where the converter is supplying DC bus power to attached loads. A negative value indicates current flow into the converter, where the converter is absorbing “regenerative” power from attached loads.
Converter Output Power
Usage | Access | T | Data Type | Default | Min | Max | Semantics of Values |
|---|---|---|---|---|---|---|---|
Optional - BD | Get | T | REAL | - | - | - | Kilowatts |
The Converter Output Power attribute is the output power generated by the Bus Converter. This value is based on the product of the Converter Output Current and DC Bus Voltage. A positive value indicates power flow out of the converter, where the converter is supplying DC bus power to attached loads. A negative value indicates power flow into the converter, where the converter is absorbing "regenerative" power from attached loads.
Provide Feedback