Induction Motor Attributes

Induction Motor Attributes

These are the motor configuration attributes that apply specifically to induction motor types.
Induction Motor Rated Frequency
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Required
Set
REAL
60
DB
0
Infinity symbol
Hertz
The Induction Motor Rated Frequency attribute is a floating point value that specifies the nameplate frequency rating of an induction motor.
Induction Motor Flux Current
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Required
Set
REAL
0
DB
FD
0
Infinity symbol
Amps (RMS)
The Induction Motor Flux Current attribute is an ID Current Reference that is required to generate full motor flux. This value is closely approximated by the No Load Motor Rated Current commonly found in Induction Motor data sheets.
Induction Motor Stator Resistance
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Required
Set
REAL
0
DB
FD
0
Infinity symbol
Ohms
The Induction Motor Stator Resistance attribute is a floating point value that specifies the Y circuit, phase-neutral, winding resistance of the stator as shown as R
1
in the IEEE motor model.
Induction Motor Stator Leakage Reactance
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Optional
Set
REAL
0
DB
FD
0
Infinity symbol
Ohms
The Induction Motor Stator Leakage Reactance attribute is a floating point value that specifies the Y circuit, phase-neutral, leakage reactance of the stator winding, at rated frequency, as shown as X
1
in the IEEE motor model.
Induction Motor Magnetization Reactance
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Optional
1
Set/
REAL
0
DB
0
Infinity symbol
Ohms
1
This parameter has a strong motor temperature component that some drives circumvent through various adaptive control or compensation techniques.
The Induction Motor Magnetization Reactance attribute is a floating point value that specifies the Y circuit, phase-neutral, magnetizing reactance of the motor, at rated frequency, as shown as X
m
in the IEEE motor model.
Induction Motor Rotor Resistance
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Optional
1
Set
REAL
0
DB
0
Infinity symbol
Ohms
1
This parameter has a strong motor temperature component that some drives circumvent through various adaptive control or compensation techniques.
The Induction Motor Rotor Resistance attribute is a floating point value that specifies the phase-neutral equivalent stator-referenced winding resistance of the rotor as shown as R
2
' in the IEEE motor model.
Induction Motor Rotor Leakage Resistance
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Optional
Set
REAL
0
DB
FD
0
Infinity symbol
Ohms
The Induction Motor Rotor Leakage Resistance attribute is a floating point value that specifies the Y circuit, phase-neutral, equivalent stator-referenced leakage inductance of the rotor winding, at rated frequency, as shown as X
2
' in the IEEE motor model.
Induction Motor Rated Slip Speed
Usage
Access
Data Type
Default
Min
Max
Semantics of Values
Optional - D
Set
REAL
0
FD
0
Infinity symbol
RPM (rotary motor type)
m/s (linear motor type)
The Induction Motor Rated Slip Speed attribute represents the amount of slip at motor rated current (full load) and motor rated frequency.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal