Equipment Sequence Diagram instructions
The table describes the
Equipment Sequence
Diagram instructions. Icon | Icon Name | Description |
Add Step and Transition Pair | Use Add Step and Transition Pair to add a step and transition pair. Although added as a pair, you can select and edit each element separately. | |
Add Disconnected Step | Use the Add Disconnected Step to add a step without adding a transition. | |
Add Disconnected Transition | Use Add Disconnected Transition to add a transition without adding a step. | |
Add Simultaneous Divergence | Use Add Simultaneous Divergence to create a branch where all linked steps execute simultaneously. | |
Add Selective Divergence | Use Add Selective Divergence to create a divergence for a selective branch. In a selective divergence, only one of multiple paths is executed--the path containing the transition that first evaluates as TRUE. | |
Add Simultaneous Convergence | Use Add Simultaneous Convergence to merge simultaneous execution paths back together. | |
Add Selective Convergence | Use Add Selective Convergence |
Provide Feedback