- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Processing Faults
The following table describes how the instruction handles execution faults:
Fault Condition | Action |
|---|---|
CVFaulted or CVEUSpanInv is set |
|
CVinitRequest | Refer to Execution. |
PV Health Bad |
|
PVFaulted is set |
|
PVSpanInv is set or SPLimitsInv is set |
|
RatioLimitsInv is set and CasRat is set and UseRatio is set |
|
TimingModeInv is set or RTSTimeStampInv is set or DeltaTInv is set |
|
Provide Feedback