Moving Average (MAVE)

Moving Average (MAVE)

This information applies to the CompactLogix 5370, ControlLogix 5570, CompactGuardLogix 5370, GuardLogix 5570, CompactGuardLogix 5380, CompactLogix 5380, CompactLogix 5480, ControlLogix 5580, and GuardLogix 5580 controllers.
The Moving Average (MAVE) instruction calculates a time average value for the In signal. This instruction optionally supports user-specified weights.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram logic.
Function Block
MAVE_FBD_avail_v31
Structured Text
MAVE(MAVE_tag,storage,weight);
Operands
Function Block
Operand
Type
Format
Description
MAVE tag
MOVING_AVERAGE
structure
MAVE structure
storage
REAL
array
Holds the moving average samples. This array must be at least as large as NumberOfSamples.
weight
REAL
array
(optional)
Used for weighted averages. This array must be at least as large as NumberOfSamples. Element [0] is used for the newest sample; element [n] is used for the oldest sample.
MOVING_AVERAGE Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
In
REAL
The analog signal input to the instruction.
Valid = any float
Default = 0.0
InFault
BOOL
Bad health indicator for the input. If In is read from an analog input, then InFault is normally controlled by fault status on the analog input. When set, InFault indicates the input signal has an error, the instruction sets the appropriate bit in Status, and the instruction holds Out at its current value. When InFault transitions from set to cleared, the instruction initializes the averaging algorithm and continues executing.
Default is cleared.
Initialize
BOOL
Initialize input to the instruction. When set, the instruction holds Out = In, except when InFault is set, in which case, the instruction holds Out at its current value. When Initialize transitions from set to cleared, the instruction initializes the averaging algorithm and continues executing.
Default is cleared.
SampleEnable
BOOL
Enable for taking a sample of In. When set, the instruction enters the value of In into the storage array and calculates a new Out value. When SampleEnable is cleared and Initialize is cleared, the instruction holds Out at its current value.
Default is set.
NumberOfSamples
DINT
The number of samples to be used in the calculation. If this value is invalid, the instruction sets the appropriate bit in Status and holds Out at its current value. When NumberOfSamples becomes valid again, the instruction initializes the averaging algorithm and continues executing.
Valid = 1 to (minimum size of StorageArray or WeightArray, if used)
Default = 1
UseWeights
BOOL
Averaging scheme input to the instruction. When set, the instruction uses the weighted method to calculate the Out. When cleared, the instruction uses the uniform method to calculate Out.
Default is cleared.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled. Cleared to false if Out overflows.
Out
REAL
The calculated output of the algorithm.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
InFaulted (Status.1)
BOOL
In health is bad (InFault is set).
NumberOfSampInv (Status.2)
BOOL
NumberOfSamples invalid or not compatible with array size.
Structured Text
Operand
Type
Format
Description
MAVE tag
MOVING_AVERAGE
structure
MAVE structure
storage
REAL
array
Holds the moving average samples. This array must be at least as large as NumberOfSamples.
weight
REAL
array
(optional)
Used for weighted averages. This array must be at least as large as NumberOfSamples. Element [0] is used for the newest sample; element [n] is used for the oldest sample.
MOVING_AVERAGE Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
Enable input. If cleared, the instruction does not execute and outputs are not updated.
Default is set.
In
REAL
The analog signal input to the instruction.
Valid = any float
Default = 0.0
InFault
BOOL
Bad health indicator for the input. If In is read from an analog input, then InFault is normally controlled by fault status on the analog input. When set, InFault indicates the input signal has an error, the instruction sets the appropriate bit in Status, and the instruction holds Out at its current value. When InFault transitions from set to cleared, the instruction initializes the averaging algorithm and continues executing.
Default is cleared.
Initialize
BOOL
Initialize input to the instruction. When set, the instruction holds Out = In, except when InFault is set, in which case, the instruction holds Out at its current value. When Initialize transitions from set to cleared, the instruction initializes the averaging algorithm and continues executing.
Default is cleared.
SampleEnable
BOOL
Enable for taking a sample of In. When set, the instruction enters the value of In into the storage array and calculates a new Out value. When SampleEnable is cleared and Initialize is cleared, the instruction holds Out at its current value.
Default is set.
NumberOfSamples
DINT
The number of samples to be used in the calculation. If this value is invalid, the instruction sets the appropriate bit in Status and holds Out at its current value. When NumberOfSamples becomes valid again, the instruction initializes the averaging algorithm and continues executing.
Valid = 1 to (minimum size of StorageArray or WeightArray, if used)
Default = 1
UseWeights
BOOL
Averaging scheme input to the instruction. When set, the instruction uses the weighted method to calculate the Out. When cleared, the instruction uses the uniform method to calculate Out.
Default is cleared.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled. Cleared to false if Out overflows.
Out
REAL
The calculated output of the algorithm.
Status
DINT
Status of the function block.
InstructFault (Status.0)
BOOL
The instruction detected one of the following execution errors. This is not a minor or major controller error. Check the remaining status bits to determine what occurred.
InFaulted (Status.1)
BOOL
In health is bad (InFault is set).
NumberOfSampInv (Status.2)
BOOL
NumberOfSamples invalid or not compatible with array size.
See Structured Text Syntax for more information on the syntax of expressions within structured text.
Description
The MAVE instruction calculates a weighted or non-weighted moving average of the input signal. The NumberOfSamples specifies the length of the moving average span. At every scan of the block when Sample Enable is set, the instruction moves the value of In into the storage array and discards the oldest value. Each In
n
has a user-configured Weight
n
, which is used if UseWeights is set.
Condition
Action
Weighted averaging method
UseWeights is set.
MAVE Weighted averaging method
Uniform averaging method
UseWeights is cleared.
MAVE_UniformAveraging_v34
The instruction will not place an invalid In value (NAN or ± INF) into the storage array. When In is invalid, the instruction sets Out = In and logs an overflow minor fault, if this reporting is enabled. When In becomes valid, the instruction initializes the averaging algorithm and continues executing.
You can make runtime changes to the NumberOfSamples parameter. If you increase the number, the instruction incrementally averages new data from the current sample size to the new sample size. If you decrease the number, the instruction recalculates the average from the beginning of the sample array to the new NumberOfSamples value.
Initializing the Averaging Algorithm
Certain conditions, such as instruction first scan and instruction first run, require the instruction to initialize the moving average algorithm. When this occurs, the instruction considers the sample StorageArray empty and incrementally averages samples from 1 to the NumberOfSamples value. For example:
MAVE Initialize average algorithm
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes for operand-related faults.
Execution
Function Block
Condition/State
Action Taken
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.EnableIn is false
Request re-initialization of Storage array the next time the instruction executes.
Tag.EnableIn is true
EnableIn and EnableOut bits are set to true.
The instruction executes.
Instruction first run
N/A
Instruction first scan
Initialize Out to zero.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal Execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table.
Example
Each scan, the instruction places input_value in array storage. The instruction calculates the average of the values in array storage, optionally using the weight values in array weight, and places the result in Out.
Function Block
MAVE_FBD_ex_v31
Structured Text
MAVE_01.In := input_value;
MAVE(MAVE_01,storage,weight);
output_value := MAVE_01.Out;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal