Flash Configuration Bad

Non-volatile configuration stored on the module is corrupted and preventing the module from operating normally.
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.