Record Low Calibration Values for Output Modules
The
Logix Designer
application commands the module to output specific levels of current. You must measure the actual level and record the results. This measurement allows the module to account for any inaccuracies.To record low calibration values for output modules:
- Measure the output values using a multimeter.
- Enter the values in the appropriateRecorded Referencebox.
- SelectNextto proceed with calibration.
- You may also selectStopto cancel the calibration.
Provide Feedback