Run Mode

The owner controller is in Run mode. The output module’s health LED will be solid green while in Run mode. If you are using an output module, newly received outputs are applied.
LED
Light Emitting Diode. It is used as a status indicator for controller functions and inputs/outputs.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.