Steps: To configure (Output State)

  1. In the
    Controller Organizer
    , right-click the module and select
    Properties
    .
  2. In the
    Module Propertie
    s dialog, select the
    Output State
    tab.
  3. Select the
    Channel
    button to select the channel to configure.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.