Unconnected
The module currently does not have a
connection open to it. The module either:
module
A device, typically an I/O device, that communicates with the controller. The controller, a particular 1756-IB16I or a PanelView are all considered modules.
connection
The link between networks and devices.
- Has not been connected to since power-up, or
- Its last connection was shut down normally and not lost via a communications fault
Provide Feedback