Fault Value outside Clamp Limits

Fault Value outside Clamp Limits

The Fault Value selected is outside the Clamp Limits. The Fault Value must be within the programmed Low Clamp Limit and High Clamp Limit.
Either Change the Low and/or High Clamp limits, or adjust the Fault Value to be between the existing Clamp Limits.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal