Failed to set the Scaling value

Failed to set the Scaling value

This error occurs when you select
OK
or
Apply
in the
PID Tag Configuration
dialog box when one of the Min or Max values in the
Scaling
tab has a maximum value that is less than the minimum value.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal