High Speed Mode

High Speed Mode

The high volume module hardware has up to four input signal connections multiplexed to one analog-to-digital (ADC) converter.
Multiple input channels are multiplexed to one analog-to-digital converter. For the highest possible conversion speed, one of those channels goes straight through to the ADC and the other three are ignored; however, faster sample rates are possible.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal