- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Import Project Documentation dialog box overview
Use the Import Project Documentation dialog box to manage the import of project documentation files.
Parameter | Description |
---|---|
Source Project | Displays the name of the project from which the localization file was generated. |
Languages to be Imported | A summary of all of the translations that will be imported from the localization file chosen in step 1 of the import wizard. The list of languages is broken up into languages that, when imported, are new to the project and languages that, when imported, will update translations that already exist in the project. This is an important distinction in that any updates to existing language translations may affect documentation already existing in the project. |
Behavior for Languages Updates | You can overwrite existing files in one of two ways:
|
Import | Click to import the localization file. |
Provide Feedback