Module Properties - SERCOS Interface
Use the SERCOS Interface tab for the:
- 1756-M03SE
- 1756-M08SE
- 1756-M16SE
- 1768-M04SE
- 1784-PM16SE
- Embedded SERCOS Interface
Use this tab to set and display the:
- SERCOS baud rate,
- update rate for the SERCOS ring, and
- fiber optic transmit power range for the SERCOS ring.
The SERCOS ring consists of the drives and axes connected to a motion module.
Parameters
Data Rate
Select the baud rate for the SERCOS ring. (For this release, this value is set to 4 MB and is Read Only.)
Cycle Time
Select the update rate for the SERCOS ring.
Transmit Power
Select the optic transmit power range for the SERCOS ring. Choose from High or Low.
Status
Displays the status the controller has about the module:
Status Name | Description |
Standby | a transient state that occurs when shutting down |
Faulted | unable to communicate with the module. When the status is Faulted, the Connection tab displays the fault. |
Validating | a transient state that occurs before connecting to the module |
Connecting | a state that occurs while the connection(s) are being established to the module |
Running | the module is communicating and everything is working as expected |
Shutting Down | the connections are closing |
Inhibited | the connection to the module is inhibited |
Waiting | a connection to this module has not yet been made due to one of the following:
|
Offline | you are not online |
OK
Click this button to accept your edits and close the dialog.
Cancel
Click this button to cancel your edits and close the dialog.
Apply
Click this button to apply your edits and continue editing.
Help
Click this button for help on this tab.
Provide Feedback