Import or export a trend

Trends can be exported to a file for storage and later analysis. Importing a trend makes it available in the Controller Organizer for viewing.
To import a trend:
  1. From the
    Controller Organizer
    , expand the
    Assets
    folder, right-click the
    Trends
    folder, and choose
    Import Trend
    .
    The
    Import Trend
    dialog is displayed.
  2. In
    File name
    , enter the name of the trend file you want to open.
    You can also enter the name by clicking on a file shown in the browser.
  3. Select
    Import
    to import the trend.
    The trend is added to the
    Trends
    folder in the
    Controller Organizer
    .
To export a trend:
  1. From the
    Controller Organizer
    , right-click the trend you want to export and choose
    Export Trend
    .
    The
    Export Trend
    dialog is displayed.
  2. In
    File name
    , enter a name for the export file.
    You do not need to add a file extension, but if you do, you must use the .L5X extension.
  3. Select
    Export
    to export the trend file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal