IntelliCENTER Dashboard

Access the IntelliCENTER Dashboard to:
  • Import a new lineup.
  • Export a lineup.
Access the
IntelliCENTER Dashboard
from the explorer bar. Select Devices Icon
Devices
, then the
IntelliCENTER
tab. Select
IntelliCENTER Dashboard
on the bottom.
On the
IntelliCENTER Dashboard
:
  • View a list of lineups and associated serial numbers.
  • Import a new lineup.
    1. Select
      Import new lineup
      .
    2. Select
      Browse
      under
      Databases
      to import datasets. Or select
      Browse
      under
      Documentation
      to import MCCs with documentation associated with it.
    3. Select one or more of the lineups and select
      Upload
      to import the datafiles into FactoryTalk Design Studio.
  • Export a lineup.
    1. Select the box associated with the lineup you want to export.
    2. Select
      Export lineup
      . The
      Export MCC Lineup
      dialog box opens.
    3. Select
      Download
      to download the zipped data set to the computer's
      Downloads
      folder.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.