Upgrade Multiple Projects
After uploading your projects to the FactoryTalk Vault, you can upgrade them to different Logix versions and different controller types.
- From the vault navigation pane, select the solution.
- From the project list, select the checkboxes for the projects you want to upgrade.
- From the vault toolbar, selectUpgrade.
- From theUpgrade Logix Projectpage in theSelect Logix Versionpull-down list, choose the version of Logix controller to upgrade to.
- Select the checkboxes for the projects to upgrade.
- (optional) In theSelect Controller Typepull-down list choose the controller catalog number to upgrade the project to.
- Review Warningsdisplays the impact of the upgrade of the project. Review the warning carefully.
- SelectUpgradeto continue with the upgrade process.
- SelectCancelto stop the upgrade process.
The status of the projects changes to
Upgrading
. Notification messages appear to inform you of the upgrade process. Once the upgrade has completed, the project status changes to Ready
if the project upgraded successfully. If problems were encountered in the upgrade, the status changes to Error
.Provide Feedback