Alternate update period not a multiple of base update period
The alternate 1 or alternate 2 or both alternate 1 and alternate 2 update periods are not a multiple of the base update period.
Choose values for the alternate update periods so that both periods are a multiple of the base update period.
Provide Feedback