Export Project Documentation dialog box overview
Use the Export Project Documentation dialog box to specify the name and location of the exported localization file.
These are the parameters for the Export Project Documentation dialog box.
Table Heading | Table Heading |
---|---|
Localization File Name | Displays an automatically generated name based on the choices you made on the previous dialog boxes of the export wizard. You may change this name. The localization file has a .txt extension. If you do not add the .txt extension to a file name, it is added for you. |
Location | The file path to the location where the localization file is to be created. The default is the default project file location or the last location used on the workstation is remembered. |
Browse | Opens the Browse for Folder to locate where you wish to export the file. |
Provide Feedback