Project Documentation not associated with a language

Attempting to import project documentation that does not have a language associated with it into a project that does have a language associated with it.
Parameters
Do not show this warning
Select this box and this warning does not display in subsequent imports.
Yes
Select this button to import the project documentation and associate the project language to the imported documentation.
No
Select this button and the project documentation is not imported into the document.
Help
Select this button for help on this warning.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.