The logic contains Pending or Accepted Edits
The
Logix Designer
application does not support the import of .L5X files with components that contain logic with pending or accepted edits. Upon export, the application warns you when this condition exists, but lets you continue with the export. However, the .L5X file cannot be imported as is.Yes
Click this button to open the Export dialog box to continue the operation.
No
Click this button to cancel the operation.
Help
Click this button for help on this dialog box.
Provide Feedback