Configure a fault routine
To execute fault-handling logic when a program fault occurs, configure a routine to be fault routine for the program. Use the
Configuration
tab of the Program Properties
dialog box to assign a fault routine.To configure a fault routine:
- From either the Controller Organizer or Logical Organizer, right-click the program to change and chooseProperties.
- Choose the routine to designate as the fault routine from theFaultmenu in theAssigned Routinesframe.
- SelectOK.
Provide Feedback