Loading
Blog
Recent ActivityRecent Activity
3 minute read

Meeting Quality Standards with Data

There are different elements that determine the quality of a final product and some of those can be tracked and shown by data collected during a batch production process.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
frozen red raspberries in sorting and processing machines

The Consumer Packaged Goods industry, like most industries, struggles to stay ahead of costs while continuing to meet quality standards and increased demands from the consumer. There are different elements that determine the quality of a final product and some of those can be tracked and shown by data collected during a batch production process.

In this blog we take a closer look at the different elements that can impact the quality of a batch and what first-step technology solution we suggest for collecting and reading process data.

Recipe maintenance

In many food and beverage facilities it is not uncommon to find recipes still kept in paper form in binders and batch data collected in spreadsheets managed by a few individuals. Add to that, the employees with decades of experience who know the recipes by heart and the quirks of machinery like the back of their hand are coming up on retirement age.

But that means if something happens to the paper recipe, or the spreadsheet gets corrupted, or deleted, valuable information is at risk. The same goes for that institutional knowledge your employees on the plant floor have; once those workers retire, where will that knowledge be stored?

Similarly in other kinds of packaged goods, like diapers, for example, there are set process steps that create the product. These steps too are often recorded on paper and stored in a binder in the facility. If anything happens to that paper, there is only the memory of the workers to rely on.

Source materials

Raw source material can vary in quality and price. Quality fluctuations may require processing changes. Running perfect batches within tolerances this month with these ingredients might not work the next month. This means different adjustments need to be made for the next batch. Setting key production indicators (KPIs) for “Golden Batch” processing looks good on paper, but the reality is more challenging with fluctuations in raw material quality.

Sampling a batch along the way takes time. Getting data on manually collected samples and manually taken readings of temperature, flow rate or pressure, leave room for error in notations or when transferring notes into a spreadsheet, and don’t consider fluctuations. Batch processing is not static, and success is dependent on many variables.

Equipment and personnel

Legacy technology is another hurdle to consistent batch production. Investing in new equipment is a significant capital expense. New equipment is considered when a facility plans to expand to meet the demand for increased flavors, and older equipment will need to keep working alongside the new equipment. It’s the long-time employees who understand best how to work with the legacy equipment. They will also know which source materials work best on which equipment. For example, raw materials that are of a lower quality might run better and produce more quality batches on older equipment than top quality ingredients do.

Depending on the raw materials available, there might be an option to run different grade levels of a product, thereby still meeting output requirements and not wasting material. Again, some of that will depend on which equipment is best suited for which outcome. In most instances, the long-term plant engineers who have worked with the equipment for years will have that information.

To avoid losing all that institutional knowledge, we suggest a digital approach that will give clearer insight into the processes you run.

Solution

When we go into food and beverage, or other types of Consumer Packaged Goods facilities, we often find inexpensive single point solutions designed to mitigate the lack of insightful data. However, those still require someone to collect the data readings from each device and enter that data in a spreadsheet. Someone will then need to run the spreadsheet reports and find the data points that indicate a problem like where a batch process went out of alignment from the preset standards.

With Batch Performance Analytics software you can gain insight into each batch process and measure the process outcomes against preset KPIs from any laptop or computer that’s running the software. With just a few keystrokes you can see fill data, process progress, and which step in the recipe the batch is at. It also means you have insight into what may need to be adjusted for the next batch to avoid going outside the established parameters.

In essence, Batch Performance Analytics identifies process gaps and indicates what can be done to correct it, such as fine-tuning recipes, pre-processing setup, refining the process steps.

Learn more here.

Published April 18, 2024

Topics: Food & Beverage FactoryTalk Batch

Jeff Botsch
Jeff Botsch
Senior Manager, Kalypso Digital Consulting
Jeff Botsch is a Senior Manager, Kalypso Digital Consulting. Recognized as a leader in digital transformation with over two decades of industry experience, Jeff specializes in crafting tailored information solutions to navigate complex manufacturing challenges. His expertise is particularly highlighted in process manufacturing across sectors such as consumer packaged goods (CPG), food & beverage, and specialty chemicals.
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Blogs Chevron RightChevron Right
  5. Chevron LeftChevron Left Meeting Quality Standards with Data Analytics Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose