Loading
The Journal | Motors and Drives

3 Ways to Improve Pump Efficiency with VFDs

Synchronization, integration and remote-visibility functions can help improve pump and compressor station performance.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
3 Ways to Improve Pump Efficiency with VFDs hero image

By Richard Paes, technical consultant for the oil and gas industry, Rockwell Automation

Using variable frequency drives (VFDs) in pipeline pump and compressor stations offers some well-established benefits related to energy savings. Drives provide the precise control needed for increasing or decreasing flow along a pipeline. The result is greater efficiency and energy savings than an across-the-line motor starter that requires control valves to manage flow.

However, with the right VFD, you can gain further benefits. Not all drive technologies are created equal, and some can help you achieve even greater cost savings and even better performance.

With this in mind, here are three key features to look for in your next pump or compressor station VFD.

1. Synchronization

A drive that supports synchronous transfer allows you to start and control several pump motors using only one drive. This can reduce your up-front capital and installation costs by as much as 33% for a two-motor system and up to 60% for a four-motor system when compared to a multiple-drive system.

A drive system with this feature also can help bring down your largest operating cost, energy usage. First, drive losses are reduced as compared to a multiple-drive system. It also allows you to bring a motor to the same frequency as the utility power supply and then transfer the motor over to that supply. This can improve overall system efficiency and provide additional energy savings.

Finally, synchronous transfer allows you to start with less impact on the power system, which will reduce or eliminate peak energy charges while also helping to prolong equipment life and reduce maintenance costs.

2. Enhanced Integration

Some modern VFDs have integration features and functions that make them easier to implement, operate and maintain.

Add-on Profiles (AOPs), for example, can simplify setup and integration by organizing drive information and configurable parameters for intuitive programming. Automatic device configuration also can streamline setup when deploying multiple drives or if you need to replace a drive. With this feature, a Logix controller stores the drive configurations and automatically downloads new or replacement drives when the controller detects them. This can help you reduce time-consuming reprogramming work.

3. Remote Visibility

When VFDs are connected to a pipeline’s control network using the correct formatting, these drives can provide actionable performance data back to a central control room. This helps operators make better decisions.

They could discover, for example, that two connected pump stations in separate energy utility zones have noticeably different rates. And they could then run the pump station harder in the zone that has lower rates. Even in a single utility zone, operators could find their energy costs are significantly lower during off-peak hours, and then adjust operations to capitalize on that lower rate.

Operators also could use the remotely accessed data to monitor and trend process performance and identify potential maintenance needs. An operator looking at three pumps running at the same speed could notice that one pump has a lower load torque. They could then send a technician to investigate the issue.

Savings

VFDs bring inherent performance and cost-savings benefits to pump and compressor stations. Choosing a VFD with synchronization, integration and remote-visibility features can take your performance and savings to a new level.

 

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Putman Media, Inc.

Topics: Drives
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left The Journal Chevron RightChevron Right
  5. Chevron LeftChevron Left 3 Ways to Improve Pump Efficiency with VFDs Chevron RightChevron Right