Loading
Magazine | Edge Computing

How Edge Computing Enhances HMI/SCADA Solutions

See how a single edge-computing platform can streamline engineering, operations and maintenance, and enhance control infrastructure efficiency & security.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Abstract concept of a face representing artificial intelligence, machine learning and Industrial Internet of Things.

Editor’s Note: This article is adapted from the white paper, “Edge Computing Creates Better HMI/SCADA Solutions

.” Download the full paper
to learn what an improved and fortified industrial control system architecture looks like; the advantages of edge computing for resolving persistent challenges; and three case studies of oil platform, ship and chemical plant control systems that transitioned to a single edge platform, modern DCS and historian software.

Traditional human-machine interface (HMI) and supervisory control and data acquisition (SCADA) architectures have served industry well for mission-critical automation control, but there is always room for improvement. With digitalization comes an edge-computing-based approach that redefines what “good” looks like in a monitoring and control system architecture.

Modern edge computing platforms solve many common challenges faced by engineers when deploying or operating HMI and SCADA in their automation and control systems.

We know that edge computing is a distributed computing framework where information is collected, processed, and stored close to the edge — where it is produced or consumed — rather than in a centralized server or data center.

Adopting edge computing within your enterprise benefits automation control, specifically HMI and SCADA design, by improving your ability to protect mission-critical operations. A single edge platform bolsters operational excellence through extensive engineering, operations and maintenance efficiencies along with critical reliability, safety and security improvements.

Keep up with industrial automation trends and technologies
weak chain representing the delicate supply chain
Subscribe to The Journal
Keep up with industrial automation trends and technologies

Subscribe to The JOURNAL from Rockwell Automation and Our PartnerNetwork's digital edition and receive the latest news and information directly to your inbox. Enter your email address and check the box for "The Journal." It's that easy!

Subscribe Now

Production Challenges

Some of the most pressing challenges with typical automation and control architectures include demand for digitalization, disparate islands of automation and downtime. Edge computing tackles these challenges by design, modernizing the infrastructure by allowing users to consolidate multiple software solutions and individual computers into a single edge platform.

Normally, HMI/SCADA software and advanced applications such as historians, manufacturing execution systems (MESs), batch, asset performance, engineering and programming software are installed in multiple computers, but edge computing with built-in virtualization avoids this complexity and cost.

In addition, a single fault-tolerant edge platform mitigates performance slowdowns caused by bandwidth and latency issues, and reduces maintenance complexities common with an otherwise rou­tinely expanding pool of hardware and software assets.

Also, edge platforms with built-in redundancy protect against unplanned downtime and support operational resilience. This is because downsizing to a single redundant device where all the automation and control software is installed increases reliability and simplifies security management, thus minimizing the risk of costly operational disruptions. Built-in redundancy and preconfigured virtualization are especially important when the SCADA or HMI is installed in a remote or hazardous environment.

White Paper
Edge Computing Creates Better HMI/SCADA Solutions

Download the white paper, “Edge Computing Creates Better HMI/SCADA Solutions,” from Stratus Technologies. Learn what an improved and fortified industrial control system architecture looks like; the advantages of edge computing for resolving persistent challenges; and three case studies of control systems from an oil platform, ship and chemical plant that benefitted from a transition to a single edge platform and a modern DCS and historian software.

Download Now

Real-World Example of Benefits

Let’s look at how a London-based chemical company benefitted from implementing an edge solution.

Synthomer transitioned to a fault-tolerant edge computing platform to centralize and optimize operations at a production plant in Italy and protect against failures and downtime. Eliminating islands of automation and standardizing the entire facility on the same system improved operational safety, resilience and analytics.

The system included:

  • Stratus ftServer
    to protect the modernized operation and house all the software used to engineer, program, operate and maintain the distributed control system (DCS).
  • Rockwell Automation PlantPAx
    ® DCS
    .
  • Rockwell Automation Allen‑Bradley® ControlLogix
    ® programmable automation controllers
    (PACs) replacing the plant’s previous disparate, multibranded programmable logic controllers (PLCs).
  • System integration performed by Progecta.

Modernizing Traditional Architectures

The depth of edge computing advantages underscores the reasons to modernize traditional automation control architectures. For mission-critical operations especially, benefits such as workload consolidation, operational resilience, downtime protection and standardization help users achieve a more powerful, efficient and secure HMI/SCADA solution.

Stratus Technologies

, based in Maynard, Massachusetts, is a Global Technology Partner in the Rockwell Automation PartnerNetworkTM program. The company provides the continuous availability of business-critical applications by delivering zero-touch edge computing platforms that are simple to deploy and maintain, protected from interruptions and threats. Stratus serves companies ranging from global Fortune 500 companies to small-to-medium sized businesses.

Like this article? Sign up for the digital magazine

(4X/year) and e-newsletter from The Journal From Rockwell Automation and Our PartnerNetwork.

 

 

The Journal From Rockwell Automation and Our PartnerNetwork™ is published by Endeavor Business Media.

Man with a tablet, virtual assistant using artificial intelligence to communicate with the cloud.
Podcast
How Edge Computing Simplifies & Enhances AI-Based Cybersecurity in IT & OT

In this episode of our “Automation Chat” podcast from The Journal From Rockwell Automation and Our PartnerNetwork magazine, Executive Editor Theresa Houck is joined by Valerie Schneider, Business Development Manager and Mike Wurster, Director of Strategic Alliances with Stratus Technologies to discuss how edge computing can enhance cybersecurity.

You’ll learn about:

• The biggest cyberthreats facing manufacturers and how to deal with them.

• How artificial intelligence can be used to enhance cybersecurity in OT environments.

• How edge computing & virtualization let users consolidate multiple applications on a single platform, allowing cybersecurity protocols to integrate with applications like HMI, SCADA, MES and batching.

• How to improve OT cybersecurity without significant investment or disruption to operations; and more.

Listen on your favorite podcast app or on the web, or watch their conversation on YouTube.

Listen Now
Watch Now
Topics: The Journal Process Solutions Smart Manufacturing PlantPAx
Recommended for You
Loading
  1. Chevron LeftChevron Left Rockwell Automation Home Chevron RightChevron Right
  2. Chevron LeftChevron Left Com... Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left The Journal Chevron RightChevron Right
  5. Chevron LeftChevron Left How Edge Computing Enhances HMI/SCADA Solutions Chevron RightChevron Right
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
You can update your preferences at any time. For more information please see our Privacy Policy
CloseClose