By Salma Ghafoor, Global Technical Lead – IOT, Rockwell Automation
I recently I found myself needing 1,000 jump rings for a project. I made a bunch of coils and then got out a pair of handheld snips and started cutting the jump rings off the coil, two or three rings at a time. It was quick and easy, and I was up and running in practically no time.
I was pretty happy with myself — for a short time anyway. After a while, my hand started to cramp, the cutters started sticking, and the whole operation slowed down to a crawl.
Soon, I’d had enough and figured I would invest in a ring-cutting machine. I researched and found one that best suited my requirements, waited for it to arrive, set it up, and, within a few minutes, I had my 1,000 jump rings. Plus, I found an unexpected advantage in that the cuts were much cleaner and flush, which increased the quality of my finished product.
Picking the Right Tool for Scalability
So, what does my ring cutting machine have to do with Industrial Internet of Things (IIoT)?
Well, the way I see it is that the IIoT can be the right tool for the job if you have a use case that you want to deploy across your entire enterprise. You can use existing tools and build something quickly; however, there’s a good chance that if you try to scale it up and out, you’ll hit a brick wall.
The IIoT encompasses many capabilities essential when building something that must scale, such as:
- Connectivity: Interact with any type of data source or system of record.
- Security: Secure and flexible authentication and authorization options to match your requirements.
- Data Model: Create common information models that correlate and contextualize data.
- Visualization: Offer intuitive and interactive dashboards for presenting the information.
- Orchestration: React to patterns in the data and create automated workflows.
- Accessibility: Control visibility and accessibility to the right people at the right time in the right format.