physicalPort object
Defines the physical port of a device.
physicalPort [busType] [name] { <property name> := <property value>; ... }
Property | Description |
---|---|
busType (required) | Type of bus the port is compatible with. |
name (required) | Name of the port. The name is automatically applied and is always A1 or A2. |
enabled | Indicates that the physical port is enabled. |
Provide Feedback