Delete the definition of an Add-On Instruction

Delete an Add-On Instruction to remove it from the project. Deleting an Add-On Instruction removes all instances from the project. Remove an Add-On Instruction from
Library
in the current project.
You cannot delete the definition of an Add-On Instruction from a project that contains instances of the Add-On Instruction. To delete the definition of an Add-On Instruction, remove all instances of the Add-On Instruction from the project.
To delete the definition of an Add-On Instruction
  1. On the explorer
    bar, select Library
    Library
    .
  2. In
    Library
    ,
    expand
    Add-On Instruction
    .
  3. Right-click the Add-On Instruction to delete and select
    Delete
    . The message
    Delete all instances of the add-on instruction from the project
    appears.
  4. Select
    Delete
    to delete the Add-On Instruction from the project, or
    Cancel
    to leave the Add-On Instruction in the project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.