Delete a project
Delete a project from the
Open project
dialog.
- Close any open project.
- Either:
- On theWelcomepage, selectOpen project.
- From the menu bar, selectFile > Open project.
- InOpen projectdialog, in theProject Namelist, hover over the project that you want to delete.
- Select the trash bin icon on the right to delete the project.
The project is only deleted from your workspace. The remote project and other user's copy of the project in their workspace will still exists.
Provide Feedback