Select a FactoryTalk Vault solution
Select a FactoryTalk Vault solution to store your converted controller project files when you create a project.
TIP:
If there is an error connecting to the Vault when creating a project, you will receive a notification to select a FactoryTalk Vault solution when pushing changes to the remote repository.
FactoryTalk Vault is a centralized solution to securely store documents, manage data access, and collaborate on projects.
- Select one of these options for a FactoryTalk Vault solution:
- Select an exiting solution
- Create solution
- SelectCreateto place your project in the FactoryTalk Vault solution.
Provide Feedback