Micro Controller Driver
Observe these guidelines when working with Micro Controller Driver.
Supported controllers
Micro Controller Driver supports
Micro800™
controllers and MicroLogix™
1400 controllers.Controller tags import
With Micro Controller Driver, you can import tags from
Micro800
controllers in the online mode.Data types
Micro Controller Driver supports these data types:
Datatype | FactoryTalk Optix datatype |
---|---|
BOOL | Boolean |
SINT | SByte |
DINT | Int32 |
REAL | Float |
STRING | String |
LREAL | Double |
INT | Int16 |
LINT | Int64 |
USINT | Byte |
BYTE | |
UINT | UInt16 |
WORD | |
UDINT | UInt32 |
DATE | |
TIME | |
DWORD | |
ULINT | UInt64 |
LWORD |
Provide Feedback