- Getting started
- Creating projects
- Graphic objects
- Predefined graphic objects
- Object and variable references
- Extending projects
- Tutorials
- Graphic objects tutorial
- NetLogic tutorial
- OPC UA tutorial
Circular gauge
Sets or displays an integer value within a range of possible values.
Use case
Set and display an analog variable value within a minimum and maximum value.
TIP:
Use the
Warning zone
property to display specific ranges of values in different colors.Example
Circular gauge with two warning zones defined

Provide Feedback