Configure a spin box
Add a spin box object and edit its properties.
- InProject view, inUI, right-click a container to contain the spin box, and then select .
- (optional) InProperties, adjust the spin box settings:
- Value. Starting value. Either a numerical value or a dynamic link to a variable with a numerical value.For more information about dynamic links, see Create dynamic links.
- Minimum value. Minimum value that you can set for the spin box.TIP: If the value is outside theMinimum valueandMaximum valuerange, the spin box border turns red for a brief moment and the value reverts to the previous value.
- Maximum value. Maximum value that you can set for the spin box.
- Increment. Value by which to increase or decrease the value when you use the buttons to increment the value.
- Input format. Format of displayed value.
- Editable. Enable entering the spin box value with keyboard keys.TIP: Even ifEditableis set toFalse, you can still use spin box buttons to increase or decrease the spin box value.
- Show buttons. Display buttons to increase or decrease the value.
Provide Feedback