Scroll view
Panel that can scroll to display content larger than the panel size.
Operation
Scroll view supports:
- Touch and multitouch gestures. Pan or pinch-to-zoom.
- Keyboard and mouse operation to zoom-in or zoom-out.or .
Use case
Display overview information, drawings, or other items that are larger than the main application container.
Example
Provide Feedback