Configure a sparkline
Configure the source of the data to display in the Sparkline object. Adjust the Sparkline object properties.
- InProject view, right-click a node to contain theSparklineobject and select .
- InProperties, create a dynamic link betweenPen valueand a node or database from which you want to obtain the data.For more information about dynamic links, see Create dynamic links.
- (optional) Configure the sparkline properties:
- Pen color. Sparkline pen color.
- Pen thickness. Sparkline pen thickness.
- Time window. Sparkline time range.
- Refresh time. Sparkline refresh time.
- Y-axis maximum. Maximum value of the Y-axis.
- Y-axis minimum. Minimum value of the Y-axis.
- Range high. High value of the range.
- Range low. Low value of the range.
- Range color. Range background color.
Provide Feedback