Add a widget to a project
You can add preconfigured widgets to a project. Use widgets to configure the FactoryTalk Optix Application at runtime, configure the device on which the application is running, and show information about the device.
NOTE:
An
OptixPanel™
project contains Date & Time
, Device
,Network
, and FT Remote Access
widgets in the Project view
by default.- From the main toolbar, selectLibraries.
- InLibraries, selectWidgets.
- Select the widget to add to the project.
- UnderComponents, complete the instructions to add the widget to the project.
- When the widget is added, inLibraries, selectClose.
The widget appears in
Project view
.
TIP:
If you add a widget that contains a node with the same name as the node that already exists in the project, the dynamic links are remapped to the node that exists in the project.
widget
Provide Feedback