Recipes editor customization
Instead of using the default recipes editor, you can design a custom recipes management interface.
TIP:
You can develop a custom recipes management interface based on the objects reused from the default recipes editor. For more information, see Reuse objects from the default recipes editor.
Graphical objects and scripts for ingredients
IMPORTANT:
While building your custom recipe management solution, you must include the objects from these NetLogic scripts.
Item | Functions | Usage |
---|---|---|
RecipesEditor object |
| In the Properties pane, in the RecipeSchema property, select a recipe schema. |
RecipesEditorUISetup NetLogic | Create the following set of objects for each ingredient of the selected recipe schema:
| To create the graphical objects, right-click RecipesEditor or RecipesEditorUISetup and select Execute Setup . |
Stored recipes selection
Item | Functions |
---|---|
RecipesComboBox object |
|
In RecipesComboBox , RecipesEditorComboBoxLogic NetLogic |
|
Recipes management
NOTE:
The following button objects invoke the respective methods of the recipe schema object.
Item | Function |
---|---|
SaveButton object | Save or update in the database the recipe written or selected in RecipesComboBox |
In SaveButton , RecipesEditorSaveButtonLogic NetLogic | |
DeleteRecipeButton object | Delete the selected recipe from the database by using RecipesComboBox |
LoadButton object | Load the selected recipe from the controller to the FTOptixApplication by using RecipesComboBox |
ApplyButton object | Apply the selected recipe on the controller by using RecipesComboBox |
Notifications
Object | Function |
---|---|
OutputMessage object | When the user saves, deletes, loads or applies a recipe, an output message displays for five seconds.
TIP:
To change the message retention time, double-click the
RecipesEditorOutputMessageLogic NetLogic script and change the value expressed in milliseconds. |
RecipesEditorOutputMessageLogic NetLogic |
customize
Provide Feedback